BridgeCurveBuilderConstraintTypes Enumeration¶
NXOpen.Features.BridgeCurveBuilder.ConstraintTypes is an alias for NXOpen.Features.BridgeCurveBuilderConstraintTypes
-
class
NXOpen.Features.
BridgeCurveBuilderConstraintTypes
¶ Bases:
object
This enum represents the end continuity constraint types for the bridge curve
Enum Members
Enum Member Enum Member Description G0 G0 continuity G1 G1 continuity G2 G2 continuity G3 G3 continuity -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-