BodyByEquationBuilderLocationTypes Enumeration¶
NXOpen.Features.BodyByEquationBuilder.LocationTypes is an alias for NXOpen.Features.BodyByEquationBuilderLocationTypes
-
class
NXOpen.Features.
BodyByEquationBuilderLocationTypes
¶ Bases:
object
The option to specify where the Symbolica or Maple worksheet exists.
Enum Members
Enum Member Enum Member Description OperatingSystem Worksheet is on the native OS file system. Teamcenter Worksheet is in Teamcenter. Embedded Worksheet is embedded in part. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-