BlockFeatureBuilderTypes Enumeration¶
NXOpen.Features.BlockFeatureBuilder.Types is an alias for NXOpen.Features.BlockFeatureBuilderTypes
-
class
NXOpen.Features.
BlockFeatureBuilderTypes
¶ Bases:
object
Represents the block types
Enum Members
Enum Member Enum Member Description OriginAndEdgeLengths Represents the block created by providing Origin and Edge Lengths TwoPointsAndHeight Represents the block created by providing Two Points and Height DiagonalPoints Represents the block created by providing Diagonal Points -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-