AssociativityType Enumeration¶
-
class
NXOpen.Features.
AssociativityType
¶ Bases:
object
Represents the associativity type for a dimension entity Enum Members
Enum Member Enum Member Description EndPoint End-point (determined from 3d help point) ArcCenter Arc-center Tangency Tangency EndPoint1 1st end point (at minimum parameter value) EndPoint2 2nd end point VerticalCenterline1 vertical centerline end point 1 VerticalCenterline2 vertical centerline end point 2 HorizontalCenterline1 horizontal centerline end point 1 HorizontalCenterline2 horizontal centerline end point 2 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-