AssociativeLineBuilderEndOption Enumeration¶
NXOpen.Features.AssociativeLineBuilder.EndOption is an alias for NXOpen.Features.AssociativeLineBuilderEndOption
-
class
NXOpen.Features.
AssociativeLineBuilderEndOption
¶ Bases:
object
Represents end options type.
Enum Members
Enum Member Enum Member Description Inferred Inferred Point Point Tangent Tangent AtAngle At angle AlongXc Along XC AlongYc Along YC AlongZc Along ZC Normal Normal -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-