AeroRibBuilderThicknessDimensionOptions Enumeration

NXOpen.Features.AeroRibBuilder.ThicknessDimensionOptions is an alias for NXOpen.Features.AeroRibBuilderThicknessDimensionOptions

class NXOpen.Features.AeroRibBuilderThicknessDimensionOptions

Bases: object

This attribute represents the options for thickness dimension

Enum Members

Enum Member Enum Member Description
Simple
Symmetric
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.