AeroRibBuilderGuideObjectTypes Enumeration¶
NXOpen.Features.AeroRibBuilder.GuideObjectTypes is an alias for NXOpen.Features.AeroRibBuilderGuideObjectTypes
-
class
NXOpen.Features.
AeroRibBuilderGuideObjectTypes
¶ Bases:
object
This attribute represents the Guide Object types
Enum Members
Enum Member Enum Member Description Face Guide object is face DatumPlane Guide object is datum plane Curve Guide object is curve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-