AeroFlangeBuilderWidthMethods Enumeration

NXOpen.Features.AeroFlangeBuilder.WidthMethods is an alias for NXOpen.Features.AeroFlangeBuilderWidthMethods

class NXOpen.Features.AeroFlangeBuilderWidthMethods

Bases: object

This attribute represents the width method

Enum Members

Enum Member Enum Member Description
OffsetGuideFace
OffsetGuideCurveAlongSkin
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.