AeroFlangeBuilderLimitObjectTypes Enumeration

NXOpen.Features.AeroFlangeBuilder.LimitObjectTypes is an alias for NXOpen.Features.AeroFlangeBuilderLimitObjectTypes

class NXOpen.Features.AeroFlangeBuilderLimitObjectTypes

Bases: object

This attribute represents the limit object types

Enum Members

Enum Member Enum Member Description
FromGuideCurve
FromSelected
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.