AdmMoveFaceBuilderMoveOptionType Enumeration¶
NXOpen.Features.AdmMoveFaceBuilder.MoveOptionType is an alias for NXOpen.Features.AdmMoveFaceBuilderMoveOptionType
-
class
NXOpen.Features.
AdmMoveFaceBuilderMoveOptionType
¶ Bases:
object
Represents the move option.
Enum Members
Enum Member Enum Member Description MoveAndAdapt Option equates to standard Move Face. CutAndPaste Option equates to enhanced Move Face with Cut or Copy Face with Paste Face and Delete Face without heal. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-