AOCSBuilderOffsetType Enumeration¶
NXOpen.Features.AOCSBuilder.OffsetType is an alias for NXOpen.Features.AOCSBuilderOffsetType
-
class
NXOpen.Features.
AOCSBuilderOffsetType
¶ Bases:
object
AOCS builder offset type enum.
Enum Members
Enum Member Enum Member Description Chordal offset_type_chordal Arclength offset_type_arclength Geodesic offset_type_geodesic Tangential offset_type_tangential Projectdistance offset_type_projectdistance -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-