AOCSBuilderFilletOptions Enumeration¶
NXOpen.Features.AOCSBuilder.FilletOptions is an alias for NXOpen.Features.AOCSBuilderFilletOptions
-
class
NXOpen.Features.
AOCSBuilderFilletOptions
¶ Bases:
object
AOCS builder fillet options type enum.
Enum Members
Enum Member Enum Member Description NoFillet No fillet Vector Vector given BestFit Best fitting ProjectedVector Use Project Vector to fillet -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-