AOCSBuilderExtend Enumeration¶
NXOpen.Features.AOCSBuilder.Extend is an alias for NXOpen.Features.AOCSBuilderExtend
-
class
NXOpen.Features.
AOCSBuilderExtend
¶ Bases:
object
AOCS builder extend to each other within section type enum.
Enum Members
Enum Member Enum Member Description NotSet no extension WithinSection allow extension -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-