FeatureProcessBuilderStatus Class¶
-
class
NXOpen.
FeatureProcessBuilderStatus
¶ Bases:
NXOpen.TransientObject
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetResultStatus | Returns a result status code for a feature process builder. |
SetResultStatus | Sets a result status code for a feature process builder. |
Enumerations¶
FeatureProcessBuilderStatusResultStatus Enumeration | Result status enumeration to indicate the result status of feature process creation |
Method Detail¶
Dispose¶
-
FeatureProcessBuilderStatus.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX7.5.0.
License requirements: None.
GetResultStatus¶
-
FeatureProcessBuilderStatus.
GetResultStatus
¶ Returns a result status code for a feature process builder.
Signature
GetResultStatus()
Returns: Return type: NXOpen.FeatureProcessBuilderStatusResultStatus
New in version NX7.5.0.
License requirements: None.
SetResultStatus¶
-
FeatureProcessBuilderStatus.
SetResultStatus
¶ Sets a result status code for a feature process builder.
Signature
SetResultStatus(result)
Parameters: result ( NXOpen.FeatureProcessBuilderStatusResultStatus
) –New in version NX7.5.0.
License requirements: None.