FeatureCollectionValidator Class¶
-
class
NXOpen.
FeatureCollectionValidator
¶ Bases:
NXOpen.TaggedObject
,NXOpen.IValidator
validator for FeatureCollection in a part.
This is a test class.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
ValidatorPrintLevel | Returns or sets the print level for validation. |
ValidatorVersion | Returns or sets the algorithm to use for validation. |
Methods¶
Method | Description |
---|---|
Destroy | Deletes the validator. |
GetValidateShape | Get the shape validation option |
SetValidateShape | Set the shape validation option |
SetValidatorPrintOodStatus | Set the ood status of features. |
Property Detail¶
ValidatorPrintLevel¶
-
FeatureCollectionValidator.
ValidatorPrintLevel
¶ Returns or sets the print level for validation.
-------------------------------------
Getter Method
Signature
ValidatorPrintLevel
Returns: Return type: NXOpen.ValidatorPrintLevel
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValidatorPrintLevel
Parameters: level ( NXOpen.ValidatorPrintLevel
) –New in version NX7.5.0.
License requirements: None.
ValidatorVersion¶
-
FeatureCollectionValidator.
ValidatorVersion
¶ Returns or sets the algorithm to use for validation.
-------------------------------------
Getter Method
Signature
ValidatorVersion
Returns: Return type: NXOpen.ValidatorVersion
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValidatorVersion
Parameters: version ( NXOpen.ValidatorVersion
) –New in version NX7.5.0.
License requirements: None.
Method Detail¶
Destroy¶
-
FeatureCollectionValidator.
Destroy
¶ Deletes the validator.
Signature
Destroy()
New in version NX7.5.0.
License requirements: None.
GetValidateShape¶
-
FeatureCollectionValidator.
GetValidateShape
¶ Get the shape validation option
Signature
GetValidateShape()
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.