AdjustMinimumRadiusBuilder Class |
Represents a NXOpen.Facet.AdjustMinimumRadiusBuilder . |
BestFitAlignBuilder Class |
This class performs the best fit alignment between objects |
BridgeFacetBodyBuilder Class |
Represents a NXOpen.Facet.BridgeFacetBodyBuilder It bridges two disjoint NX facet bodies. |
CleanupFacetBodyBuilder Class |
Represents a NXOpen.Facet.CleanupFacetBodyBuilder builder. |
CombineFacetBodyBuilder Class |
Represents a NXOpen.Facet.CombineFacetBodyBuilder builder. |
ConvertFacetBodyBuilder Class |
Represents a NXOpen.Facet.ConvertFacetBodyBuilder builder. |
CreateTransitionBuilder Class |
Represents a NXOpen.Facet.CreateTransitionBuilder builder. |
CurvatureBuilder Class |
Represents a NXOpen.Facet.CurvatureBuilder . |
DecimateFacetBodyBuilder Class |
Represents a NXOpen.Facet.DecimateFacetBodyBuilder . |
DetectPrimitivesBuilder Class |
This class manages the primitive shape detection for a facet body. |
DivideFacetFaceBuilder Class |
Represents a NXOpen.Facet.DivideFacetFaceBuilder . |
ExtrudeFacetBodyBuilder Class |
Represents a NXOpen.Facet.ExtrudeFacetBodyBuilder It extrudes a NX Facet Body. |
ExtrudeProfileBuilder Class |
Represents a NXOpen.Facet.ExtrudeProfileBuilder It extrudes 3D closed profile between planes. |
FacetBodyFromBodyBuilder Class |
Represents a NXOpen.Facet.FacetBodyFromBodyBuilder builder. |
FacetModelingCollection Class |
Collection of freeform facet operations. |
FacetedBody Class |
Represents a faceted body. |
FacetedBodyCollection Class |
Represents a collection of faceted bodies in a part |
FacetedEdge Class |
Represents a faceted edge. |
FacetedFace Class |
Represents a faceted face. |
FeatureExtractionBuilder Class |
Represents a NXOpen.Facet.FeatureExtractionBuilder It extracts feature lines or separates regions of different curvature from a facet body based on the curvature map. |
FillHoleBuilder Class |
This class finds and fills holes to a prescribed boundary smoothness condition. |
LocalOffsetBuilder Class |
Represents a NXOpen.Facet.LocalOffsetBuilder . |
MergeFacetBodyBuilder Class |
Represents a NXOpen.Facet.MergeFacetBodyBuilder It merges two overlapping NX facet bodies. |
MergeFacetFacesBuilder Class |
Represents a Facet.MergeFacetFacesBuilder builder |
MultiPatchAlignmentBuilder Class |
Aligns multiple facet bodies to one another without using reference points. |
PaintBrushBuilder Class |
This class manages the paint brush utility for a facet body. |
PaintFacetBodyBuilder Class |
This class manages the color painting on a facet body. |
PolygonModelingBuilder Class |
Represents a NXOpen.Facet.PolygonModelingBuilder builder. |
RemoveUndercutsBuilder Class |
This class handles the removal of undercut regions of a facet body. |
STLImportBuilder Class |
The STL file import builder. |
SelectFacetedBody Class |
Represents a single object selection. |
SelectFacetedBodyList Class |
Represents a list of objects on a selection list. |
SewFacetBodyBuilder Class |
Represents a NXOpen.Facet.SewFacetBodyBuilder It sews two touching NX facet bodies. |
SmoothFacetBodyBuilder Class |
Represents a NXOpen.Facet.SmoothFacetBodyBuilder . |
SnipFacetBodyBuilder Class |
Represents a SnipFacetBody builder |
SubdivideFacetBodyBuilder Class |
This class provides functionality to subdivide the polygons to increase the density of the facet bodies. |