SubdivideFacetBodyBuilderSubdivisionMethodType Enumeration¶
NXOpen.Facet.SubdivideFacetBodyBuilder.SubdivisionMethodType is an alias for NXOpen.Facet.SubdivideFacetBodyBuilderSubdivisionMethodType
-
class
NXOpen.Facet.
SubdivideFacetBodyBuilderSubdivisionMethodType
¶ Bases:
object
Subdivision methods
Enum Members
Enum Member Enum Member Description SubdivideIntoFour Subdivides the polygons into four sub triangles. The original mesh structure remains. SubdividebyEdgeLength Subdivides the polygons to a specified edge length. The original mesh structure disappears. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-