STLImportBuilderSTLFileUnitsTypes Enumeration

NXOpen.Facet.STLImportBuilder.STLFileUnitsTypes is an alias for NXOpen.Facet.STLImportBuilderSTLFileUnitsTypes

class NXOpen.Facet.STLImportBuilderSTLFileUnitsTypes

Bases: object

The STL file units types

Enum Members

Enum Member Enum Member Description
Meters
Millimeters
Inches
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.