PolygonModelingBuilder Class¶
-
class
NXOpen.Facet.
PolygonModelingBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Facet.PolygonModelingBuilder
builder.To create a new instance of this class, use
NXOpen.Facet.FacetModelingCollection.CreatePolygonModelingBuilder()
Default values.
Property Value ConvertType Convergent New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
ConvertType | Returns or sets the convert type |
SelectFacetBodies | Returns the selected bodies |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
MergeAllFaces | Merges all faces of the input body |
RemoveParameterOfBody | Removes the parameters of the input body |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PolygonModelingBuilderConvertTypes Enumeration | the conversion type |
Property Detail¶
ConvertType¶
-
PolygonModelingBuilder.
ConvertType
¶ Returns or sets the convert type
-------------------------------------
Getter Method
Signature
ConvertType
Returns: Return type: NXOpen.Facet.PolygonModelingBuilderConvertTypes
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConvertType
Parameters: convertType ( NXOpen.Facet.PolygonModelingBuilderConvertTypes
) –New in version NX12.0.0.
License requirements: nx_polygon_modeling (” NX Polygon Modeling”)
SelectFacetBodies¶
-
PolygonModelingBuilder.
SelectFacetBodies
¶ Returns the selected bodies
-------------------------------------
Getter Method
Signature
SelectFacetBodies
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX12.0.0.
License requirements: None.
Method Detail¶
MergeAllFaces¶
-
PolygonModelingBuilder.
MergeAllFaces
¶ Merges all faces of the input body
Signature
MergeAllFaces(bodyTag)
Parameters: bodyTag ( NXOpen.Body
) –New in version NX12.0.0.
License requirements: nx_polygon_modeling (” NX Polygon Modeling”)
RemoveParameterOfBody¶
-
PolygonModelingBuilder.
RemoveParameterOfBody
¶ Removes the parameters of the input body
Signature
RemoveParameterOfBody(bodyTag)
Parameters: bodyTag ( NXOpen.Body
) –New in version NX12.0.0.
License requirements: nx_polygon_modeling (” NX Polygon Modeling”)
Validate¶
-
PolygonModelingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.