LocalOffsetBuilderTransitionMethodType Enumeration¶
NXOpen.Facet.LocalOffsetBuilder.TransitionMethodType is an alias for NXOpen.Facet.LocalOffsetBuilderTransitionMethodType
-
class
NXOpen.Facet.
LocalOffsetBuilderTransitionMethodType
¶ Bases:
object
Transition Region Definition
Enum Members
Enum Member Enum Member Description NotSet None creates an offset without a transition region. ByConstantOffset Constant offset creates a transition region of constant distance. ByRegionSelection Region selection allows the user to select transtion regions. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-