FillHoleBuilderTypes Enumeration¶
NXOpen.Facet.FillHoleBuilder.Types is an alias for NXOpen.Facet.FillHoleBuilderTypes
-
class
NXOpen.Facet.
FillHoleBuilderTypes
¶ Bases:
object
Hole filling type options.
Enum Members
Enum Member Enum Member Description FillHole Fills individual hole(s). FillIsland Fills a hole defined by inner island and outer facet body. BridgeGap Bridges some open boundary edges with a linear fill. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-