FillHoleBuilderTargetTypes Enumeration¶
NXOpen.Facet.FillHoleBuilder.TargetTypes is an alias for NXOpen.Facet.FillHoleBuilderTargetTypes
-
class
NXOpen.Facet.
FillHoleBuilderTargetTypes
¶ Bases:
object
Options defining how to target holes for filling.
Enum Members
Enum Member Enum Member Description UserDefined Fills user-defined target holes. ByNumberOfEdges Automatically target holes based on number of edges. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-