FeatureExtractionBuilderInputActions Enumeration¶
NXOpen.Facet.FeatureExtractionBuilder.InputActions is an alias for NXOpen.Facet.FeatureExtractionBuilderInputActions
-
class
NXOpen.Facet.
FeatureExtractionBuilderInputActions
¶ Bases:
object
Specifies how to handle the input facet bodies.
Enum Members
Enum Member Enum Member Description Blank Blank the input facet bodies Retain Retain the input facet bodies Delete Delete the input facet bodies -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-