FacetedFaceFacetedfaceType Enumeration¶
NXOpen.Facet.FacetedFace.FacetedfaceType is an alias for NXOpen.Facet.FacetedFaceFacetedfaceType
-
class
NXOpen.Facet.
FacetedFaceFacetedfaceType
¶ Bases:
object
Facet Face type
New in version NX8.5.1.
Enum Members
Enum Member Enum Member Description Undefined Undefined body type Planar Planar face Cylindrical Cylindrical face Conical Conical face Spherical Spherical face Toroidal Face from toroid Parametric Parametric face -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-