ExtrudeFacetBodyBuilderLimitType Enumeration¶
NXOpen.Facet.ExtrudeFacetBodyBuilder.LimitType is an alias for NXOpen.Facet.ExtrudeFacetBodyBuilderLimitType
-
class
NXOpen.Facet.
ExtrudeFacetBodyBuilderLimitType
¶ Bases:
object
Represents the extrude limit type
Enum Members
Enum Member Enum Member Description Distance Specify the limit by direction and distance. Direction and Distance need to be specified. ToPlane Specify the limit by plane object. Plane needes to be specified. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-