DivideFacetFaceBuilderDivideFacetTypes Enumeration¶
NXOpen.Facet.DivideFacetFaceBuilder.DivideFacetTypes is an alias for NXOpen.Facet.DivideFacetFaceBuilderDivideFacetTypes
-
class
NXOpen.Facet.
DivideFacetFaceBuilderDivideFacetTypes
¶ Bases:
object
Divide Facet Face type
Enum Members
Enum Member Enum Member Description ByRegion Divide Facet face based on selected regional facets ByColor Divide Facet face based on colored facets -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-