CleanupFacetBodyBuilderOriginalBodyOptions Enumeration¶
NXOpen.Facet.CleanupFacetBodyBuilder.OriginalBodyOptions is an alias for NXOpen.Facet.CleanupFacetBodyBuilderOriginalBodyOptions
-
class
NXOpen.Facet.
CleanupFacetBodyBuilderOriginalBodyOptions
¶ Bases:
object
These represent the options for handling the input bodies
Enum Members
Enum Member Enum Member Description Keep Keep original body Hide Hide original body Delete Delete original body -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-