CleanupFacetBodyBuilderCleanupOptions Enumeration¶
NXOpen.Facet.CleanupFacetBodyBuilder.CleanupOptions is an alias for NXOpen.Facet.CleanupFacetBodyBuilderCleanupOptions
-
class
NXOpen.Facet.
CleanupFacetBodyBuilderCleanupOptions
¶ Bases:
object
These represent the options for each facet defect
Enum Members
Enum Member Enum Member Description NotSet Don’t perform Analysis or Repair Analyze Perform Analysis Repair Perform Repair -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-