BridgeFacetBodyBuilderSmoothTypes Enumeration¶
NXOpen.Facet.BridgeFacetBodyBuilder.SmoothTypes is an alias for NXOpen.Facet.BridgeFacetBodyBuilderSmoothTypes
-
class
NXOpen.Facet.
BridgeFacetBodyBuilderSmoothTypes
¶ Bases:
object
Represents the smoothness type for the inserted new facets
Enum Members
Enum Member Enum Member Description Linear Insert new facets with linear smoothness TangentBased Insert new facets with tangent smoothness -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-