BestFitAlignBuilderConstraintOptions Enumeration¶
NXOpen.Facet.BestFitAlignBuilder.ConstraintOptions is an alias for NXOpen.Facet.BestFitAlignBuilderConstraintOptions
-
class
NXOpen.Facet.
BestFitAlignBuilderConstraintOptions
¶ Bases:
object
Represents the constraint options
Enum Members
Enum Member Enum Member Description Free No constraint OnlyTranslation Only translation TranslationInPlane Translation in the plane TranslationAlongDirection Translation along direction OnlyRotation Only rotation RotationAroundPoint Rotation around specific point RotationAroundLine Rotation around specific line HoldToPlane Moving in the plane HoldToLine Moving along the line -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-