ExtrudeTaperDataTaperType Enumeration¶
-
class
NXOpen.
ExtrudeTaperDataTaperType
¶ Bases:
object
This enum represents the type of taper Enum Members
Enum Member Enum Member Description NotSet No taper SimpleFromStart Simple taper from start edges SimpleFromProfile Simple taper from profile Symmetric Symmetric taper MatchedEnds Matched end taper Asymmetric ASymmetric taper -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-