EffectivityConditionBuilderToUnitType Enumeration¶
NXOpen.EffectivityConditionBuilder.ToUnitType is an alias for NXOpen.EffectivityConditionBuilderToUnitType
-
class
NXOpen.
EffectivityConditionBuilderToUnitType
¶ Bases:
object
Specifies option for range effectivity value’s toUnit. This enumeration is valid only for the effectivity type
NXOpen.EffectivityConditionBuilderEffectivityConditionType.UnitRange
Enum Members
Enum Member Enum Member Description StockOut Sets stock out unit as toUnit effectivity range OpenEnd Sets open end unit as toUnit for effectivity range -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-