EdgeSheetBoundaryRule Class¶
-
class
NXOpen.
EdgeSheetBoundaryRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects boundary edges of a sheet body.New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the edge sheet boundary rule: NXOpen.EdgeSheetBoundaryRule |
Method Detail¶
Dispose¶
-
EdgeSheetBoundaryRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetData¶
-
EdgeSheetBoundaryRule.
GetData
¶ Gets the data for the edge sheet boundary rule:
NXOpen.EdgeSheetBoundaryRule
Signature
GetData()
Returns: Sheet body whose boundary edges are used to create this rule Return type: NXOpen.Body
New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)