EdgeEdgeType Enumeration¶
NXOpen.Edge.EdgeType is an alias for NXOpen.EdgeEdgeType
-
class
NXOpen.
EdgeEdgeType
¶ Bases:
object
Solid edge type.
Enum Members
Enum Member Enum Member Description Rubber Rubber edge, no curve attached Linear Linear edge Circular Circular edge Elliptical Elliptical edge Intersection Intersection edge Spline Spline edge SpCurve SP curve edge Foreign Foreign edge ConstantParameter Constant parameter edge TrimmedCurve Trimmed curve edge Convergent Convergent edge Undefined Undefined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-