EdgeDumbRule Class¶
-
class
NXOpen.
EdgeDumbRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects edges without any intent i.e. as if collected with Single Curve rule. .. versionadded:: NX3.0.0
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the edge dumb rule: NXOpen.EdgeDumbRule |
Method Detail¶
Dispose¶
-
EdgeDumbRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetData¶
-
EdgeDumbRule.
GetData
¶ Gets the data for the edge dumb rule:
NXOpen.EdgeDumbRule
Signature
GetData()
Returns: Edges which creates edge dumb rule Return type: list of NXOpen.Edge
New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)