EdgeChainRule Class¶
-
class
NXOpen.
EdgeChainRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects end-to-end connected edges from the body of the seed edge.New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the edge chain rule: NXOpen.EdgeChainRule |
Method Detail¶
Dispose¶
-
EdgeChainRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetData¶
-
EdgeChainRule.
GetData
¶ Gets the data for the edge chain rule:
NXOpen.EdgeChainRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (startEdge, endEdge, isFromStart) startEdge is a
NXOpen.Edge
. Start edge of edge chain. endEdge is aNXOpen.Edge
. End edge of edge chain. isFromStart is a bool. True: the chain starts from the start point of the start edge .. versionadded:: NX3.0.0License requirements: gateway (“UG GATEWAY”)