EdgeBodyRule Class¶
-
class
NXOpen.
EdgeBodyRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects all the edges of a body.New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the edge body rule: NXOpen.EdgeBodyRule |
Method Detail¶
Dispose¶
-
EdgeBodyRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetData¶
-
EdgeBodyRule.
GetData
¶ Gets the data for the edge body rule:
NXOpen.EdgeBodyRule
Signature
GetData()
Returns: Body whose edges are used to create this rule Return type: NXOpen.Body
New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)