DxfdwgCreatorExportSplinesAsOptions Enumeration¶
NXOpen.DxfdwgCreator.ExportSplinesAsOptions is an alias for NXOpen.DxfdwgCreatorExportSplinesAsOptions
-
class
NXOpen.
DxfdwgCreatorExportSplinesAsOptions
¶ Bases:
object
Export Faces As option
Enum Members
Enum Member Enum Member Description Spline Polyline2D export faces as facets Polyline3D export faces as polyline mesh -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-