NXOpen.Drawings Package

Classes

AddObjectsToRegionBuilder Class Creates the builder for associating the symbols from library to the region
AddRemoveBoxViewBuilder Class This class is used to construct the add remove box view Builder
AnnotationSettingsBuilder Class Represents a Drawings.AnnotationSettingsBuilder.
AssociativeAngleBuilder Class This builder allows the user to create an associative or non-associative angle by measuring between a combination of two objects or vectors evaluated on a specified plane, or by an expression
AutomationBookletBuilder Class Represents a NXOpen.Drawings.AutomationBookletBuilder
AutomationTemplateRegionBuilder Class Represents a NXOpen.Drawings.AutomationTemplateRegionBuilder
BaseHalfSectionLine Class Represents a Base Half Section Line.
BasePointToPointSectionLine Class Represents a Base Point to Point Section Line.
BaseSteppedSectionLine Class Represents a Base Stepped Section Line.
BaseView Class Represents a Base View.
BaseViewBuilder Class Represents a NXOpen.Drawings.BaseView builder
BaseViewStyle Class Represents set of Base View Style Preferences applicable to drafting views.
BorderAndZoneStyleBuilder Class Represents the Border and Zone Style Builder which manages all the style attributes related * to sheet borders, sheet margins and sheet zones.
BordersAndZones Class Represents Borders and Zones
BordersAndZonesBuilder Class Builder for creating Borders and Zones.
BordersAndZonesCollection Class Represents a collection of NXOpen.Drawings.BordersAndZones objects
BrokenViewBuilder Class This class is used to construct the broken view Builder
CompareReportBuilder Class Represents a NXOpen.Drawings.CompareReportBuilder builder
ConversionProcessSettingsBuilder Class Represents a Drawings.ConversionProcessSettingsBuilder.
ConvertDraftingContentsBuilder Class Represents a Drawings.ConvertDraftingContentsBuilder.
ConvertToPMIBuilderManager Class Represents NXOpen.Drawings.ConvertToPMIBuilderManager
CustomViewSettingsBuilder Class this class represents the this class represents Drawings.
DetailView Class Represents a Detail View.
DetailViewBuilder Class Represents a NXOpen.Drawings.DetailView.
DraftingBody Class Represents a drafting body.
DraftingBodyCollection Class Represents a collection of :py:class:`NXOpen.Drawings.DraftingBody`s.
DraftingComponentSelectionBuilder Class This builder allows the user to select a view in which component objects can be designated as primary or secondary geometry
DraftingCurve Class Represents a Drafting VD Curve.
DraftingCurveCollection Class Represents a collection of :py:class:`NXOpen.Drawings.DraftingCurve`s.
DraftingCurveInfo Class Represents Drafting Curve Info
DraftingDrawingSheet Class Represents a drafting drawing sheet.
DraftingDrawingSheetBuilder Class Represents a Builder for creating :py:class:`NXOpen.Drawings.DraftingDrawingSheet`s
DraftingDrawingSheetCollection Class Represents a collection of :py:class:`NXOpen.Drawings.DraftingDrawingSheet`s.
DraftingPoint Class Represents a Drafting VD Point.
DraftingPointCollection Class Represents a collection of :py:class:`NXOpen.Drawings.DraftingPoint`s.
DraftingView Class Represents a drafting view.
DraftingViewCollection Class Represents a collection of :py:class:`NXOpen.Drawings.DraftingView`s.
DrawingCompareSettingsBuilder Class Represents a NXOpen.Drawings.DrawingCompareSettingsBuilder builder
DrawingFormatSheetBuilder Class Represents a NXOpen.Drawings.DrawingFormatSheetBuilder
DrawingRegion Class Represents a Drawing Region
DrawingRegionBuilder Class Represents a Drawing Region Builder
DrawingRegionCollection Class Represents a collection of drawing regions
DrawingRegionRulesBuilder Class Represents a Drawing region rules builder
DrawingSheet Class Represents a drawing sheet.
DrawingSheetBuilder Class Represents a NXOpen.Drawings.DrawingSheetBuilder
DrawingSheetCollection Class Represents a collection of drawing sheets.
DrawingView Class Drawing View - an empty view created without any geometric objects.
DrawingViewBuilder Class This builder allows the user to create a Drawing View
DrawingsPropertiesBuilder Class Represents an NXOpen.Drawings.DrawingsPropertiesBuilder to be used for marking the component as secondary geometry.
EditSectionLineSettingsBuilder Class Represents a NXOpen.Drawings.EditSectionLineSettingsBuilder builder.
EditViewLabelSettingsBuilder Class Represents a NXOpen.Drawings.EditViewLabelSettingsBuilder builder.
EditViewSettingsBuilder Class Represents a NXOpen.Drawings.EditViewSettingsBuilder builder.
FlatPatternObject Class Provides an interface to the data available for flat pattern objects on drawing views.
FlatPatternViewStyle Class Provides access to object and callout properties for sheet-metal data in flat pattern views on drawings.
GeneralViewStyle Class Represents set of General View Styles Preferences applicable to drafting views.
GeneralWorkFlowBuilder Class Represents a NXOpen.Drawings.GeneralWorkFlowBuilder
HalfPictorialSectionLine Class Half Pictorial Section Line is used to create a pictorial view with half of the part sectioned and the other half un-sectioned.
HalfSectionLine Class Half Section Line is used to create a view with half of the part sectioned and the other half un-sectioned.
HalfSectionLineBuilder Class Represents a NXOpen.Drawings.HalfSectionLineBuilder.
HiddenLinesViewStyle Class Represents set of Hidden Lines View Style Preferences applicable to drafting views.
HiddenObjectsBuilder Class This builder allows the user to select a view in which component objects can be designated as hidden or shown
HingeLineBuilder Class Represents a Drawings.
InheritPmiViewStyle Class Represents set of InheritPmiViewStyle applicable to drafting views.
MarkAsTemplateBuilder Class Represents a NXOpen.Drawings.MarkAsTemplateBuilder
MultipleViewPlacementBuilder Class This builder allows the user to create a Multiple View Placement
OrderManager Class Represents an object that manages orders.
OrientationViewStyle Class Represents set of Orientation View Style Preferences applicable to drafting views.
OrientedSectionLine Class Represents a Oriented Section Line.
OrientedSectionLineBuilder Class Represents a NXOpen.Drawings.OrientedSectionLineBuilder.
OvtBuilder Class Represents a NXOpen.Drawings.OvtBuilder
ParentViewBuilder Class Represents a NXOpen.Drawings.ParentViewBuilder.
PerspectiveViewStyle Class Represents set of PerspectiveViewStyle applicable to drafting views.
PictorialSectionLine Class A Pictorial Simple or Pictorial Stepped Section Line.
PointAndAngleSectionLine Class Point and Angle Section Line lets you create a view with multiple segment cuts with no bends.
PointAndAngleSectionLineBuilder Class Represents a NXOpen.Drawings.PointAndAngleSectionLineBuilder.
PointToPointSectionLine Class Point to Point Section Line lets you create a view with multiple segment cuts with no bends.
PointToPointSectionLineBuilder Class Represents a NXOpen.Drawings.PointToPointSectionLineBuilder.
ProjectedView Class Represents a Projected View.
ProjectedViewBuilder Class Represents a NXOpen.Drawings.ProjectedView builder
ProjectedViewOrientationBuilder Class Represents a NXOpen.Drawings.ProjectedViewOrientationBuilder
ProjectedViewStyle Class Represents set of Projected View Style Preferences applicable to drafting views.
RefineDisplayBuilder Class Represents a NXOpen.Drawings.RefineDisplayBuilder.
RemoveObjectsBuilder Class Creates the builder for removing associated objects from the region
RenderSet Class Represents a RenderSet.
ReportBuilder Class Represents a Drawings.ReportBuilder.
RevolvedSectionLine Class Revolved Section Line is used to create section views which are revolved about an axis.
RevolvedSectionLineBuilder Class Represents a NXOpen.Drawings.RevolvedSectionLineBuilder.
SecondaryGeometryInViewsBuilder Class This builder allows the user to select existing view(s) in which component objects can be designated as secondary or primary
SectionInViewBuilder Class This builder allows the user to select a view in which component or solid body objects can be designated as section, non-sectioned, or neither
SectionLine Class Represents a Section Line.
SectionLineBuilder Class Represents a NXOpen.Drawings.SectionLineBuilder.
SectionLineCollection Class Represents a collection of :py:class:`NXOpen.Drawings.SectionLine`s.
SectionLineSegmentBuilder Class Represents a NXOpen.Drawings.SectionLineSegmentBuilder.
SectionLineSegmentBuilderList Class Represents a list of objects.
SectionLineSegmentPointBuilder Class Represents Section Line Segment Point Builder
SectionLineSegmentPointListBuilder Class Represents SectionLineSegmentPointListBuilder class.
SectionLineSegmentsBuilder Class Represents a class Drawings.
SectionLineSettingsBuilder Class Represents the Section Line Settings Builder (Drawings.
SectionLineStyleBuilder Class Represents a Drawings.
SectionView Class Represents a Section View.
SectionViewBuilder Class Represents a NXOpen.Drawings.SectionView builder
SectionViewStyle Class Represents set of Section View Style Preferences applicable to drafting views.
SelectDraftingView Class Represents a single object selection.
SelectDraftingViewList Class Represents a list of objects on a selection list.
SelectDrawingRegion Class Represents a single object selection.
SelectDrawingView Class Represents a single object selection.
SelectDrawingViewList Class Represents a list of objects on a selection list.
SelectModelViewBuilder Class Represents a Select Model View builder that selects a model view
SelectRegionBuilder Class Creates the builder for associating the objects from the screen
SelectSectionLine Class Represents a single object selection.
SettingsBuilder Class Represents a Drawings.SettingsBuilder.
ShadingViewStyle Class Represents set of Shading View style applicable to drafting views.
SheetBorderSettingsBuilder Class Represents a NXOpen.Drawings.SheetBorderSettingsBuilder.
SheetDraftingViewCollection Class Represents a collection of :py:class:`NXOpen.Drawings.DraftingView`s.
SheetMarginSettingsBuilder Class Represents the Drawing Sheet Margins Style Builder.
SheetSectionLineCollection Class Represents a collection of :py:class:`NXOpen.Drawings.SectionLine`s.
SheetTemplateManager Class Represents a manager of :py:class:`NXOpen.Drawings.DraftingView`s.
SheetZoneReferenceBuilder Class builder for creating sheet zone refernce control strings based on the selected attribute and view
SheetZoneSettingsBuilder Class Represents the Drawing Sheet Zone Setting Style Builder.
ShipDraftingViewLinesBuilder Class Represents a ship view lines block
ShipDraftingViewLinesBuilderList Class Represents a list of objects.
ShipDraftingViewLinesViewStyle Class Represents set of Ship Drafting Lines View Style applicable to drafting views.
ShipbuildingLinesViewStyle Class Represents set of Shipbuilding Lines View Style applicable to drafting views.
SketchSectionLineBuilder Class Represents a Drawings.SectionLine builder
SketchedHalfSectionLine Class Sketched Half Section Line is sketch based section line.
SketchedPointToPointSectionLine Class Sketched Point to Point Section Line is sketch based section line.
SketchedSteppedSectionLine Class A Sketched Simple or Stepped Section Line is sketch based section line.
SmoothEdgesViewStyle Class Represents set of Smooth Edges View Style Preferences applicable to drafting views.
SpecifySectionLineBuilder Class Select a section line
StandardViewsBuilder Class This builder allows the user to create a Drawing View
SteppedSectionLine Class A Simple or Stepped Section Line.
SteppedSectionLineBuilder Class Represents a NXOpen.Drawings.SteppedSectionLineBuilder.
SvtBuilder Class Represents a NXOpen.Drawings.SvtBuilder
ThreadsViewStyle Class Represents set of Threads View Style Preferences applicable to drafting views.
TraceLinesViewStyle Class Represents interface for Trace Lines View Style Preferences applicable to drafting views.
TrackDrawingChangesGeneralBuilder Class Represents a NXOpen.Drawings.TrackDrawingChangesGeneralBuilder
TrackDrawingChangesReportFilterBuilder Class Represents a Drawings.TrackDrawingChangesReportFilterBuilder
UpdateViewsBuilder Class Represents a NXOpen.Drawings.UpdateViewsBuilder
View2dOrientBuilder Class Represents the View 2D Orientation (Drawings.
ViewAlignment Class View Alignment object.
ViewAlignmentBuilder Class Represents a NXOpen.Drawings.ViewAlignmentBuilder.
ViewAlignmentCollection Class Represents a collection of :py:class:`NXOpen.Drawings.ViewAlignment`s.
ViewBoundaryBuilder Class Represents the View Boundary (Drawings.
ViewBreak Class ViewBreak - defines the portion of a view that gets hidden to produce a broken view
ViewBreakBuilder Class Represents a NXOpen.Drawings.ViewBreakBuilder
ViewBreakCollection Class Represents a collection of :py:class:`NXOpen.Drawings.ViewBreak`s.
ViewCenterCoordinateBuilder Class Represents the View center coodinate (Drawings.
ViewCommonViewLabelBuilder Class Represents a NXOpen.Drawings.ViewCommonViewLabelBuilder
ViewCopyTo3dBuilder Class Represents a NXOpen.Drawings.ViewCopyTo3dBuilder.
ViewCreationWizardBuilder Class This builder allows the user to create a Drawing View
ViewDetailLabelBuilder Class Represents a NXOpen.Drawings.ViewDetailLabelBuilder
ViewLabelBuilder Class Represents a NXOpen.Drawings.ViewLabelBuilder
ViewOrientationBuilder Class Represents a ViewOrientationBuilder.
ViewPlacementBuilder Class Represents a NXOpen.Drawings.ViewPlacementBuilder.
ViewProjectedArrowSettingsBuilder Class Represents a NXOpen.Drawings.ViewProjectedArrowSettingsBuilder
ViewProjectedLabelBuilder Class Represents a NXOpen.Drawings.ViewProjectedLabelBuilder
ViewProjectedViewSettingsBuilder Class Represents a NXOpen.Drawings.ViewProjectedViewSettingsBuilder
ViewProjectionBuilder Class Represents a NXOpen.Drawings.ViewProjectionBuilder.
ViewProjectionPlaneBuilder Class Represents the View Projection Plane (Drawings.
ViewScaleBuilder Class Represents the View Scale (Drawings.
ViewSectionLabelBuilder Class Represents a NXOpen.Drawings.ViewSectionLabelBuilder
ViewSectionLineBuilder Class Represents a NXOpen.Drawings.ViewSectionLineBuilder
ViewSettingsBuilder Class Represents a Drawings.ViewSettingsBuilder.
ViewStyle Class Represents set of style applicable to drafting views.
ViewStyleBaseBuilder Class Represents the BASE tab on the View Style Dialog (Drawings.
ViewStyleBuilder Class Represents the View Style Builder (Drawings.
ViewStyleDetailBuilder Class Represents the DETAIL tab on the View Style Dialog (Drawings.
ViewStyleFPCalloutConfigBuilder Class Represents the Callout section of the Flat Pattern tab on the View Style Dialog (Drawings.
ViewStyleFPCalloutsBuilder Class Represents the Callout section of the Flat Pattern tab on the View Style Dialog (Drawings.
ViewStyleFPCurvesBuilder Class Represents the Curve section of the Flat Pattern tab on the View Style Dialog (Drawings.
ViewStyleGeneralBuilder Class Represents view style general builder (Drawings.
ViewStyleHiddenLinesBuilder Class Represents the HIDDEN LINES tab on the View Style Dialog (Drawings.
ViewStyleInheritPmiBuilder Class Represents the INHERIT PMI tab on the View Style Dialog (Drawings.
ViewStyleOrientationBuilder Class Represents the ORIENTATION tab on the View Style Dialog (Drawings.
ViewStylePerspectiveBuilder Class Represents the PERSPECTIVE tab on the View Style Dialog (Drawings.
ViewStyleProjectedBuilder Class Represents the PROJECTED tab on the View Style Dialog (Drawings.
ViewStyleSecondaryComponentsBuilder Class Represents the Secondary Geometry tab on the View Style Dialog (Drawings.
ViewStyleSectionBuilder Class Represents the SECTION tab on the View Style Dialog (Drawings.
ViewStyleSectionConstraintsBuilder Class Represents the SECTION CONSTRAINTS tab on the View Style Dialog (Drawings.
ViewStyleShadingBuilder Class Represents the SHADING tab on the View Style Dialog (Drawings.
ViewStyleShipbuildingLinesBuilder Class Represents the Shipbuilding LINES tab on the View Style Dialog (Drawings.
ViewStyleShipbuildingLinesBuilderList Class Represents a list of objects.
ViewStyleSmoothEdgesBuilder Class Represents the SMOOTH EDGES tab on the View Style Dialog (Drawings.
ViewStyleThreadsBuilder Class Represents the THREADS tab on the View Style Dialog (Drawings.
ViewStyleTraceLinesBuilder Class Represents the TRACE LINES tab on the View Style Dialog (Drawings.
ViewStyleVirtualIntersectionsBuilder Class Represents the VIRTUAL INTERSECTIONS tab on the View Style Dialog (Drawings.
ViewStyleVisibleLinesBuilder Class Represents the VISIBLE LINES tab on the View Style Dialog (Drawings.
ViewWorkflowBuilder Class Represents a NXOpen.Drawings.ViewWorkflowBuilder
ViewingDirectionArrow Class This class represents a Drafting Viewing Direction Arrow.
ViewingDirectionArrowLabel Class This class represents a Drafting Viewing Direction Arrow Label.
VirtualIntersectionsViewStyle Class Represents set of Virtual Intersections View Style Preferences applicable to drafting views.
VisibleAndHiddenLinesColorFontWidthBuilder Class Represent a NXOpen.Drawings.VisibleAndHiddenLinesColorFontWidthBuilder
VisibleLinesViewStyle Class Represents set of Visible Lines View Style Preferences applicable to drafting views.
VisualDrawingComparePrefsBuilder Class This class gets and sets components of Visual Overlay in Drafting Preferences.

Enumerations

AddRemoveBoxViewBuilderModeType Enumeration Mode type
AnnotationSettingsBuilderAnnotationTypeEnum Enumeration enum is used to list out annotation types
AnnotationSettingsBuilderUnitsEnum Enumeration enum is used to list out different unit types
ArrowDirectionType Enumeration the arrow direction type
ArrowStyleType Enumeration the arrow style type
AssociativeAngleBuilderEvaluationPlaneType Enumeration evaluation plane types
AssociativeAngleBuilderObjectType Enumeration Represents the object type.
BordersAndZonesBuilderFontEnum Enumeration the font
BordersAndZonesBuilderHorizontalCenteringMarkType Enumeration the horizontal centering mark type
BordersAndZonesBuilderVerticalCenteringMarkType Enumeration the vertical centering mark type
BordersAndZonesBuilderZoneMethod Enumeration the zone method
BordersAndZonesBuilderZoneOrigin Enumeration the zone origin
BrokenViewBuilderBreakLineStyle Enumeration Break Line Type
BrokenViewBuilderHorizontalBreakSide Enumeration Which side to remove in case of vertical single-sided break.
BrokenViewBuilderLineWidth Enumeration Line Width
BrokenViewBuilderTypeBreak Enumeration Specifies whether the break is two-sided (regular) or one-sided.
BrokenViewBuilderTypeDirection Enumeration Direction Enum
BrokenViewBuilderVerticalBreakSide Enumeration Which side to remove in case of horizontal single-sided break.
ConversionProcessSettingsBuilderActionOnErrorEnum Enumeration enum is used to list out different Action on error types
ConvertDraftingContentsBuilderSelectConversionEntityType Enumeration enum is used to list out different entity that can be use for conversion
CustomViewSettingsBuilderFeatures Enumeration the options for small features
CustomViewSettingsBuilderFont Enumeration the options for all the fonts used in the custom view settings dialog
CustomViewSettingsBuilderInterfering Enumeration the options for interfering curves
CustomViewSettingsBuilderThreadStandards Enumeration the thread standards options
CustomViewSettingsBuilderWidth Enumeration the width options for all the line width used in the customize view settings dialog
DetailViewBuilderLabelOnParentType Enumeration the display type for the label on parent
DetailViewBuilderTypes Enumeration the type of boundary
DraftingComponentSelectionBuilderGeometry Enumeration type of geometry
DraftingCurveInfoDraftingCurveType Enumeration Specifies the drafting curve types
DraftingViewCollectionViewCopyAnnotOption Enumeration Specifies the the annotation copy mode.
DraftingViewCollectionViewCopyDetailOption Enumeration Specifies the the view copy mode.
DraftingViewCollectionViewUpdateOption Enumeration Specifies which drafting views to update.
DrawingCompareSettingsBuilderChangeSymbolType Enumeration Represents a Compare Settings Change symbol Types
DrawingCompareSettingsBuilderComparisonBaseline Enumeration Represents a Compare Settings ComparisonBaseline
DrawingCompareSettingsBuilderFontType Enumeration Represents a Compare Settings Change symbol font types
DrawingCompareSettingsBuilderWidthType Enumeration Represents a Compare Settings Change symbol width types
DrawingRegionBuilderContentToMove Enumeration Specifies the region content to move
DrawingRegionBuilderRegionContinuation Enumeration Specifies the region continuation type
DrawingRegionBuilderRegionDraftingObjectType Enumeration Specifies the drafting object type
DrawingRegionBuilderRegionGrowthDirection Enumeration Specifies the region growth direction (this is for NXOpen.Annotations.CustomSymbol and NXOpen.Annotations.Note)
DrawingRegionBuilderRegionHorizontalGrowthDirection Enumeration Specifies the region horizontal growth direction
DrawingRegionBuilderRegionVerticalGrowthDirection Enumeration Specifies the region vertical growth direction
DrawingSheetProjectionAngleType Enumeration Specifies the projection angle of a drawing sheet.
DrawingSheetStandardSheetSize Enumeration Standard Drawing sizes
DrawingSheetUnit Enumeration Specifies the units of the drawing sheet.
DrawingSheetBuilderSheetBaseordrawingView Enumeration the base view or drawing view option
DrawingSheetBuilderSheetMode Enumeration the drawing sheet dialog mode
DrawingSheetBuilderSheetOption Enumeration the options for specifying the attributes of the new drawing sheet to be created.
DrawingSheetBuilderSheetProjectionAngle Enumeration the drawing sheet projection angle
DrawingSheetBuilderSheetStandardEnglishScale Enumeration the standard English drawing sheet scales
DrawingSheetBuilderSheetStandardMetricScale Enumeration the standard Metric drawing sheet scales
DrawingSheetBuilderSheetUnits Enumeration the drawing sheet units
DrawingsPropertiesBuilderSecondaryComponentOptions Enumeration Options for managing the secondary geometry property on the components
FontEnum Enumeration the font
GeneralWorkFlowBuilderGridSettingsType Enumeration Represents the grid settings type.
GeneralWorkFlowBuilderModelBasedAlwaysStartType Enumeration Represents the always start type.
GeneralWorkFlowBuilderSettingsOrientationType Enumeration Represents the settings orientation type.
HingeLineBuilderHingeline Enumeration Specifies the hinge line vector option
HorizontalCenteringMarkType Enumeration the horizontal centering mark type
LabelPositionTypes Enumeration label position type
LetterFormatTypes Enumeration letter format type
MarkAsTemplateBuilderActionTypeEnum Enumeration the action type enum.
MarkAsTemplateBuilderItemTypeEnum Enumeration the item type enum.
MarkAsTemplateBuilderRelationTypeEnum Enumeration the relation type enum.
MarkAsTemplateBuilderTemplateTypeEnum Enumeration the template type enum.
Method Enumeration the zone method
MultipleViewPlacementBuilderOption Enumeration The placement option type
ReferenceShowTypes Enumeration reference show type
RotationSymbolTypes Enumeration Rotation symbol types
ScalePositionTypes Enumeration scale Position type
ScaleValueFormatTypes Enumeration scale value format type
SectionInViewBuilderEditSxtype Enumeration Edit Section type
SectionLineBuilderTypes Enumeration Section Line type
SectionLineSegmentBuilderTypes Enumeration the point
SectionLineSegmentPointBuilderSegmentTypes Enumeration Section Segment Types
SectionLineStyleBuilderArrowheadStyleType Enumeration This enum represents arrowhead style type.
SectionLineStyleBuilderCreateSectionLineType Enumeration This enum represents whether or not to create a view for the section line.
SectionLineStyleBuilderFontStyle Enumeration This enum represents section line font style type.
SectionLineStyleBuilderLabelLocationStyle Enumeration This enum represents section line label location for ISO128 section lines.
SectionLineStyleBuilderStandardStyle Enumeration This enum represents section line standard style type.
SectionLineStyleBuilderWidthStyle Enumeration This enum represents section line width style type.
SectionViewBuilderSectionCutType Enumeration Section Line Cut type
SectionViewBuilderSectionLineType Enumeration Section Line type
SectionViewBuilderSectionViewModeType Enumeration Section Line Mode
ShipDraftingViewLinesViewStyleLines Enumeration Line type
ShipbuildingLinesViewStyleLines Enumeration Line type
ShipbuildingLinesViewStyleShipbuildingLines Enumeration Geometry type
SketchSectionLineBuilderSectionLineTypes Enumeration Section line type
SketchSectionLineBuilderType Enumeration Section type
StandardViewsBuilderPlacement Enumeration The view Layout placement type (deprecated)
StandardViewsBuilderType Enumeration The view Layout type
StandardViewsBuilderView Enumeration The view type to create
TrackDrawingChangesGeneralBuilderBaselineOfComparisonType Enumeration Represents baseline Of comparison type
TrackDrawingChangesGeneralBuilderCompareMethodType Enumeration Represents compare method type
TrackDrawingChangesGeneralBuilderSnapshotDataToUseType Enumeration Represents snapshot data to use type
TrackDrawingChangesGeneralBuilderSymbolType Enumeration Represents symbol type
TrackDrawingChangesReportFilterBuilderFilter Enumeration Represents Report Filter options
TrimmingMarkStyleType Enumeration the trimming mark style type
VerticalCenteringMarkType Enumeration the vertical centering mark type
View2dOrientBuilderCustomMethod Enumeration The custom orientation method
View2dOrientBuilderType Enumeration The view orientation type
ViewBoundaryBuilderType Enumeration The view boundary type
ViewBreakBuilderViewbreaklinestyle Enumeration style for view break line
ViewCommonViewLabelBuilderSecondaryAlignmentType Enumeration secondary Alignment Type
ViewCommonViewLabelBuilderSecondaryIndexingType Enumeration secondary Indexing Type
ViewCopyTo3dBuilderBoundingBoxOption Enumeration The bounding box options
ViewCopyTo3dBuilderDistanceFromViewPlaneOption Enumeration The option to get the distance
ViewCopyTo3dBuilderOption Enumeration The pre-NX7.
ViewCopyTo3dBuilderOutputOption Enumeration The output options
ViewCopyTo3dBuilderTypes Enumeration The type of copy to 3d selections
ViewCreationWizardBuilderOption Enumeration The placement option type
ViewCreationWizardBuilderResolutionOption Enumeration the view resolution option type
ViewCreationWizardBuilderViewBoundaryOption Enumeration The view boundary option type
ViewCreationWizardBuilderViewRepresentations Enumeration the view representation mode
ViewDetailLabelBuilderLabelParentDisplayTypes Enumeration Label on Parent Display type
ViewDetailLabelBuilderLabelParentTextPlacement Enumeration Label on Parent Text Placement type
ViewLabelTypes Enumeration view label type
ViewOrientationBuilderOrientation Enumeration This enum represents view orientation type.
ViewPlacementBuilderMethod Enumeration view method
ViewPlacementBuilderOption Enumeration view option
ViewProjectedArrowSettingsBuilderDimensionsStyleType Enumeration Represents arrowhead style
ViewProjectedArrowSettingsBuilderDispalyLabelType Enumeration Represents display label type
ViewProjectedViewSettingsBuilderDisplayArrowOnParentViewType Enumeration Represents display arrow on parent view
ViewProjectionBuilderCurveType Enumeration the value of curve type in the setting group
ViewProjectionBuilderTypes Enumeration the type of view projection
ViewProjectionPlaneBuilderPlaneOptions Enumeration the plane options to select
ViewScaleBuilderType Enumeration The view scale type
ViewSectionLineBuilderDisplayType Enumeration specifies the section line symbol display
ViewSectionLineBuilderLocationType Enumeration specifies the label location for ISO128 section lines.
ViewSectionLineBuilderShowSectionLineType Enumeration specifies the show section line options
ViewSectionLineBuilderStyleType Enumeration specifies the section line arrowhead style
ViewSettingsBuilderRenderingStyleEnum Enumeration enum is used to list out different rendering style types
ViewStyleFPCalloutConfigBuilderOrientationType Enumeration This enum represents orientation types for the flat pattern callouts
ViewWorkflowBuilderDisplay Enumeration Represents the extracted edge face display option
ViewWorkflowBuilderHandlingBodiesType Enumeration Represents option for handling bodies with no valid lightweight data
ViewWorkflowBuilderHandlingbodies Enumeration Represents option for handling bodies with no valid lightweight data
ViewWorkflowBuilderSplarcs Enumeration Represents the setting for splarcs geometry projected as arc option
ViewWorkflowBuilderStyle Enumeration Represents the preview stle option
VisualDrawingComparePrefsBuilderVisualDrawingComparePrefsMethodType Enumeration Compare Method Type This indicate various options of Compare Method.
VisualDrawingComparePrefsBuilderVisualDrawingComparePrefsOverlayDataToUse Enumeration Overlay Data To Use This indicate various options that can be used before Overlaying
ZoneOrigin Enumeration the zone origin