VisualDrawingComparePrefsBuilderVisualDrawingComparePrefsMethodType Enumeration¶
NXOpen.Drawings.VisualDrawingComparePrefsBuilder.VisualDrawingComparePrefsMethodType is an alias for NXOpen.Drawings.VisualDrawingComparePrefsBuilderVisualDrawingComparePrefsMethodType
-
class
NXOpen.Drawings.
VisualDrawingComparePrefsBuilderVisualDrawingComparePrefsMethodType
¶ Bases:
object
Compare Method Type This indicate various options of Compare Method.
Enum Members
Enum Member Enum Member Description AgainstAnotherDrawing This option is used to overlay different part over current part AgainstOverlayDatainActiveDrawing This option is used to overlay current part on itself -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-