ViewSectionLineBuilderStyleType Enumeration

NXOpen.Drawings.ViewSectionLineBuilder.StyleType is an alias for NXOpen.Drawings.ViewSectionLineBuilderStyleType

class NXOpen.Drawings.ViewSectionLineBuilderStyleType

Bases: object

specifies the section line arrowhead style

Enum Members

Enum Member Enum Member Description
Open
Closed
Filled
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.