ViewSectionLineBuilderShowSectionLineType Enumeration

NXOpen.Drawings.ViewSectionLineBuilder.ShowSectionLineType is an alias for NXOpen.Drawings.ViewSectionLineBuilderShowSectionLineType

class NXOpen.Drawings.ViewSectionLineBuilderShowSectionLineType

Bases: object

specifies the show section line options

Enum Members

Enum Member Enum Member Description
WithSectionView
WithoutSectionView
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.