ViewSectionLineBuilderLocationType Enumeration

NXOpen.Drawings.ViewSectionLineBuilder.LocationType is an alias for NXOpen.Drawings.ViewSectionLineBuilderLocationType

class NXOpen.Drawings.ViewSectionLineBuilderLocationType

Bases: object

specifies the label location for ISO128 section lines.

Enum Members

Enum Member Enum Member Description
OnArrow
OnEnd
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.