ViewProjectionPlaneBuilderPlaneOptions Enumeration¶
NXOpen.Drawings.ViewProjectionPlaneBuilder.PlaneOptions is an alias for NXOpen.Drawings.ViewProjectionPlaneBuilderPlaneOptions
-
class
NXOpen.Drawings.
ViewProjectionPlaneBuilderPlaneOptions
¶ Bases:
object
the plane options to select
Enum Members
Enum Member Enum Member Description Inferred Inferred plane from vector, point and plane view DepthValue Get plane using source view and depth value -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-