ViewProjectedViewSettingsBuilderDisplayArrowOnParentViewType Enumeration

NXOpen.Drawings.ViewProjectedViewSettingsBuilder.DisplayArrowOnParentViewType is an alias for NXOpen.Drawings.ViewProjectedViewSettingsBuilderDisplayArrowOnParentViewType

class NXOpen.Drawings.ViewProjectedViewSettingsBuilderDisplayArrowOnParentViewType

Bases: object

Represents display arrow on parent view

Enum Members

Enum Member Enum Member Description
No
NonOrtho
All
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.