ViewPlacementBuilderOption Enumeration¶
NXOpen.Drawings.ViewPlacementBuilder.Option is an alias for NXOpen.Drawings.ViewPlacementBuilderOption
-
class
NXOpen.Drawings.
ViewPlacementBuilderOption
¶ Bases:
object
view option
Enum Members
Enum Member Enum Member Description ToView Align to the view centers ModelPoint Align to the same point in the alignment view and the view being edited PointToPoint Align a point in the alignment view to another point in the view being edited -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-