ViewPlacementBuilderMethod Enumeration¶
NXOpen.Drawings.ViewPlacementBuilder.Method is an alias for NXOpen.Drawings.ViewPlacementBuilderMethod
-
class
NXOpen.Drawings.
ViewPlacementBuilderMethod
¶ Bases:
object
view method
Enum Members
Enum Member Enum Member Description Infer Infer the view position Horizontal Align the view horizontally to another view Vertical Align the view vertically to another view PerpendicularToLine Align the view along some line to another view Overlay Align the view on top of another view PerpendicularToHingeLine Align the view along the hinge line Max Should be the last enum in the list -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-