ViewBreakCollection Class

class NXOpen.Drawings.ViewBreakCollection

Bases: object

Represents a collection of :py:class:`NXOpen.Drawings.ViewBreak`s.

To obtain an instance of this class, refer to NXOpen.Drawings.DraftingView

New in version NX7.5.0.

Methods

Method Description
FindObject Finds the NXOpen.Drawings.DraftingView with the given identifier as recorded in a journal.

Method Detail

FindObject

ViewBreakCollection.FindObject

Finds the NXOpen.Drawings.DraftingView with the given identifier as recorded in a journal.

An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.

An exception will be thrown if no object can be found with the given journal identifier.

Signature FindObject(journalIdentifier)

Parameters:journalIdentifier (str) – Identifier of the drafting view to be found
Returns:View with this identifier
Return type:NXOpen.Drawings.ViewBreak

New in version NX7.5.0.

License requirements: None.