TrackDrawingChangesReportFilterBuilder Class¶
-
class
NXOpen.Drawings.
TrackDrawingChangesReportFilterBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
Drawings.TrackDrawingChangesReportFilterBuilder
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
GetReportFilterStatus | Returns report filter status |
SetReportFilterStatus | Sets report filter status |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TrackDrawingChangesReportFilterBuilderFilter Enumeration | Represents Report Filter options |
Method Detail¶
GetReportFilterStatus¶
-
TrackDrawingChangesReportFilterBuilder.
GetReportFilterStatus
¶ Returns report filter status
Signature
GetReportFilterStatus(reportFilterType)
Parameters: reportFilterType ( NXOpen.Drawings.TrackDrawingChangesReportFilterBuilderFilter
) –Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
SetReportFilterStatus¶
-
TrackDrawingChangesReportFilterBuilder.
SetReportFilterStatus
¶ Sets report filter status
Signature
SetReportFilterStatus(reportFilterType, reportFilterStatus)
Parameters: - reportFilterType (
NXOpen.Drawings.TrackDrawingChangesReportFilterBuilderFilter
) – - reportFilterStatus (bool) –
New in version NX11.0.0.
License requirements: drafting (“DRAFTING”)
- reportFilterType (
Validate¶
-
TrackDrawingChangesReportFilterBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.