TrackDrawingChangesGeneralBuilderCompareMethodType Enumeration¶
NXOpen.Drawings.TrackDrawingChangesGeneralBuilder.CompareMethodType is an alias for NXOpen.Drawings.TrackDrawingChangesGeneralBuilderCompareMethodType
-
class
NXOpen.Drawings.
TrackDrawingChangesGeneralBuilderCompareMethodType
¶ Bases:
object
Represents compare method type
Enum Members
Enum Member Enum Member Description AgainstAnotherDrawing This option is used to compare different part over current part AgainstSnapshotDataInActiveDrawing This option is used to compare current part on itself OpenSavedComparisonReport This option is used to open a compare report that is saved in the current part -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-